Email_Header_2550x130px_Banner_Automate

HOT PRESS STAMPING

hot-form-oven-tools-1

HOT PRESS STAMPING FOR SHEET METAL FORMING

PROCESSES & PRODUCTS FOR YOUR AUTOMATION APPLICATIONS

The hot stamping process takes lightweight material, hardeneds and strengthens it to form needed shaped parts. Hot Stamping (metal forming, metal stamping), is mostly used in the automotive industry – to form pieces of steel or aluminum into car components/parts. This includes structural components like vehicle doors, frames, hoods, pillars, etc. DESTACO's End Effectors are designed and built to touch, hold and handle the steel and/or aluminum that can be inserted or placed in various types of hot stamping ovens or furnaces, heating the material in excess of 900 degrees C. and also to retrieve the hot stamped parts from the ovens and place them where needed.

Types of Hot Stamping Ovens

There are two types of hot stamping ovens: Soak Oven and Stack Oven. We grab the blank and place it into a soak oven where conveyors moves parts and increase the parts' temperatures, and then our grippers place them into a die for stamping. For the inside die, fluid cools the item before coming out.

Contact us today to share your project goals and technical specifications with our applications engineers!

hot-form-grippers-1

AUTOMATING YOUR PRESS ROOM APPLICATIONS

In the Metal Stamping industries, there are common styles of Press Lines that parts are formed on - Progressive, Transfer, Tandem. Progressive Press Lines run smaller parts and do not require automation or tooling to move parts from die to die. Transfer Press Lines have 3 Axis Transfer Rails (Mechanical or Servo) where automation tooling (Finger Tooling) is mounted and used to transfer the part from die to die. Transfer Presses have either Mechanical Transfer or Servo Transfer Systems. Mechanical Transfer have a fixed motion relative to the Press Ram timing, where as Servo Transfers motion is not limited to fixed motion, allowing for custom motions of transfer rails to be optimized for maximum throughput. Tandem Line Presses will have multiple Press in a row. In a Tandem Line, there can be between 4 to 7 Presses. The Press tending or part transfer in Tandem lines may have simple 3 Axis Pick and Place Systems or a number of 6 Axis Robots that Load/Unload parts into or out of the presses.
press-unload-2

AUTOMATION TOOLING & END EFFECTORS

Stamped parts are not always completed parts. Some stampings may need to be welded or assembled to an additional stamping. Metal Assembly is a highly automated part of an automotive plant. Automation Tooling and Robotic End-of-Arm Tooling (EOAT) play a very important role in the success and efficiency of a Metal Assembly Process.

Automation Tooling (aka Finger Tooling) describes the solution utilized in a Transfer Press application to transfer the part. It will consist of a gripper and shovel or some combination of the two. Finger Tooling will include the gripper or shovel back, modular tooling and, the attachment point of a Transfer Rail. The attachment point will have utilities (i.e. Air Supply and Electrical) to operate the Finger Tool.

End effectors (also known as End-of-Arm Tooling, or "EOAT") are devices attached to the end of a robotic arm. They act as the robot’s “hand” and are the portion of the solution that contacts the part being transferred.

DESTACO provides solutions for all areas of sheet metal forming and automation, including:

Assembly, CNC Machining, Press room/ stamping, Hot Forming, Welding

View
Application
Group

End effectors (also known as End-of-Arm Tooling, or "EOAT") are devices attached to the end of a robotic arm. They act as the robot’s “hand” and are the portion of the solution that contacts the part being transferred.

DESTACO provides solutions for all areas of sheet metal forming and hot press stamping, including:

Back to Top